Hamburg, 17 October 2016. Electro-technology specialists Pfannenberg will be presenting communication-enabled thermal management devices for electrical enclosures at the SPS IPC Drives show in Nuremberg [...] installation. Compact cooling units Compact cooling units for the standard range from 1,000 to 1,500 W in the e Cool family will be on display for the first time. Their power, and their compact [...] chillers in the Compact series are available in two sizes offering between them six power levels from 1 kW to 6.6 kW. They are of a particularly space-saving design. With this range of power levels, it is