592 SP - 13347-390 Indaiatuba +55 19 3935-7187 +55 19 3935-7187 service@pfannenberg.com.br www.pfannenberg.com.br [...] Service Adresses Pfannenberg provides full service for chillers and cooling units for electrical enclosures from all manufacturers. Download: Pfannenberg Global Service Contacts address list Europe, Middle
system with visualization and the dashboard. Standard signaling towers such as the BR35 and the BR50 with an Asi module which display the current machine status and issue warning signals in [...] ent and is available at no cost on-line. The compact water/glycol chiller PC 2500 and the EB 95 9.5 kW chiller will also be displayed at the stand. [...] is easily possible, by entering the coolant and filling quantity noted on the type plate of every chiller, to determine whether there is an urgent need for action. The calculator uses this data to find the
is opened for example, are displayed in real time on an external screen. Compact chillers The new chillers in the Compact series are available in two sizes offering between them six power levels [...] in the areas where their machines operate. For example, using the modular signaling towers BR50 and BR35 wherever there is a requirement to display machine statuses and provide warning signals, [...] monitoring can deliver and find out about the benefits it offers users. The latest cooling units and chillers can provide a wide range of relevant data which users can use for predictive maintenance, for example
y after moulding. Chillers tailored to the needs of specific applications are particularly suitable for the demanding task of cooling injection moulding machines. Chiller configuration precisely matched [...] avoid underdimensioning or overdimensioning of the chiller. A good example of what a tailored package solution looks like is the Pfannenberg chiller installed in the test lab of PolymerEngineering in Hamburg [...] basic conditions, the objective was to cool all three machines with a single chiller. In order to determine the right chiller for the job, Pfannenberg’s experts first analysed the local conditions and
the EB series chillers allow economic system solutions which work independently of the ambient air. Typical areas of application are filling lines and packaging systems. Pfannenberg chillers – with cooling [...] Starting from the compactly designed, highly efficient and easy to service standard unit, this chiller can be equipped with several additional features to match specific applications. For example, all [...] The EB devices are UL certified and can be used at ambient temperatures from -20 °C to +45 °C. All chillers in the range allow users to benefit from lower energy and operating costs, space-saving installation
opening of the cabinet door. New application-specific chiller systems Another highlight at the stand is the updated energy-efficient chiller , which is part of the EB 2.0 series. With revamped case [...] 16 kW. The new design with a full metal enclosure makes it easier for manufacturers to design the chillers into their machines. An integrated microchannel condenser also reduces the required refrigerant [...] service personnel. In addition, Pfannenberg offers customers the option of application-specific chiller design directly on site. Top-mounted cooling units: more space and lower cost With regard