In 2018, the world's largest trade fair for interactive entertainment is celebrating its tenth anniversary with "Light it up! 10 years of Gamescom", a spectacular lighting installation. Art Illumination by Hamburg light artist Michael Batz creates a breath-taking showcase for lots of the city’s famous buildings. Some eye-catching examples are the 85m tall Messeturm in Deutz, the Hohenzollern Bridge, the main railway station, the Cologne Tower, the Messehochhaus, as well as various hotels, buildings, ships on the Rhine and other bridges. Around 600 QUADRO R flashing lights from Pfannenberg are being used at the Messeturm.
The fair and the Art Illumination end on the 25th of August.