purely visual display on a signaling tower only provides a snapshot of machine status. If the status changes, valuable data is lost for the want of recordings and analysis tools. Pfannenberg Signal Analytics [...] dashboard also visualizes in 2D the entire manufacturing area and allows signals and data to be configured. At the stand at SPS UPC Drives, PSA will be exhibited as a system with visualization and the dashboard [...] the multifunction QUADRO LED-HI light and the ABL LED-HI and ABS LED-HI signalinglights for large halls and spaces will also be exhibited. Outdoor cooling devices for extreme environments
Categories of signalingtechnology Flashing lights LED lights Function monitored Safety related lights Accessories Certified with EN 54-23! With the European standard EN 54-23 taking effect from 1 January 2014 [...] Visualsignaling. Pfannenberg visualsignaling devices ensure any process and alarm status can be displayed safely at any time. Benefit from top quality standards and a unique complete range. Categories [...] alarm systems, additional visible signaling which comply with the EN 54-23 requirements and have the necessary certification are mandatory. Pfannenberg’s flashing light PY X-S-05 in the standardised lens
above all economically. Continue Reading Xenon or LED: the application decides the technology Two different technologies are usually considered in the choice of lights for a signaling application: LED and [...] solution. Continue Reading or Download as PDF Fire protection in accordance with VDE 0833-2: changes relating to visualsignaling devices in fire alarm systems The provisions of the standard for visual signaling [...] Technical Reports SignalingTechnology Software-supported planning and dimensioning of signaling devices in fire alarm systems The right fire alarm can save lives. Especially in industry a well and efficiently
counterpart in the Gleinalm Tunnel in Austria. Continue reading or download as PDF. Hekatron Application EN 54-23 – Increased requirements made to visualsignaling devices mean that special attention must be [...] just products. Audible fire alarm systems in logistics centres Application Pfannenberg equips the distribution hub at one of world's largest online retailers with audible signaling devices. Continue reading [...] select the correct products in the respective application. Continue reading or download as PDF. EXPO 2015 Application Fire alarm devices protecting over 21 million visitors. Continue reading or download
areas of signalingtechnology… Read more LED or Xenon? How to find the right technology for informing, warning or alerting. Read more Functional Safety - SIL/PL Safety-related sounders/flashing lights for a [...] flashing lights and sounders for industrial applications with special requirements. Read more Technical Reports SignalingTechnology Individual reports with detailed background information on signaling technology [...] are your partner for all questions regarding signalingtechnology. Learn more about standard compliant and efficient dimensioning, as well as about products and solutions that meet specific requirements
warning, alarm Indication – Warning – Alarm VisualSignaling Audible Signaling Combined SignalingSignal Towers Ex-Atex Signaling Obstacle lights M12 plug signaling devices Art Illumination Accessories PATROL [...] combined visual/audible devices for industrial use. PATROL stands for Pfannenberg's Advanced Technology Range Of Loudness. It provides a range of sounder and combined visual/audible signaling devices for [...] Visit our new beta version product pages Test now Indication – Warning – Alarm Service partner for visual & audible signals. Indication – Warning – Alarm Global competition pushes the automation of industrial
solely an audible signal has been installed, an additional visualsignal must be used. With the EN 54-23 taking effect, demands are also being made regarding the light output and light distribution. The [...] g. production facilities). Light colour The visualsignaling device must emit white or red flashing light. Flash rate The flash rate must be between 0.5 Hz and 2 Hz. Coverage volume Visual alarm devices [...] EN 54-23 certified flashing lights from Pfannenberg In most European countries EN 54-23 has taken effect in 2013 for visualsignaling devices. Pfannenberg was the first manufacturer to offer beacons that
signaling, alerting and thermal management support the production processes with outstanding performance levels. Modern and innovative signalingtechnology. Signalingtechnology is faced with a variety [...] For example, our BR 50 signal tower: modular in construction – it signals the particular conditions and hazardous situations using a continuouslight, flashing light, blinking light or sound. Via an AS-i [...] Continuous excellence for the production process. Rapid cycle sequences are a major feature in the manufacturing and packaging of food and beverage products. Our specific components and solutions for signaling
individual needs. The increased light output is provided by powerful, replaceable LEDs, which can also determine the signaling mode. Continuous, blinking or flashing signaling modes in six different colours [...] BR 50 signal tower can be used wherever machine statuses need to be indicated or warning signals need to be given. It impresses with its flexibility and with outstanding perceptibility: The signal tower [...] The new M12 variant makes handling even easier Visual-, audible or combination signaling devices in all performance classes - all these signaling solutions can already be integrated even faster into
the Quadro LED-HI has three different signal options - continuouslight, flashing and strobe light. In combination with numerous possible hood colours, the signaling device for industrial applications can [...] develop an optimal signaling solution for the required application," says René Jarvers, Sales Expert SignalingTechnology at Pfannenberg. In addition to the industrial signaling devices and personal [...] reliable perceptibility of signals for signaling crane statuses. The crane manufacturer BANG Kransysteme GmbH & Co. KG relies on the powerful QUADRO LED-HI multifunctional lights from Pfannenberg for its