Case Study
Swiss Krono Group - It‘s all about the cut-out.
Cut-out-compatible cooling solutions from Pfannenberg reduce maintenance requirements and improve machine availability for the Swiss Krono Group, producers of engineered wood products based in Heiligengrabe, Germany.
Large amounts of dust in the air are a particular challenge for electronic components and cooling systems for electrical enclosures used in the wood engineering industry. In the search for a solution which would prevent machine failure caused by heavy soiling and would also guarantee rapid retrofitting, the Swiss Krono Group chose the cut-out compatible thermal management concept from Pfannenberg.
"The people from Pfannenberg first presented their thermal management concept and then over the following weeks pointed out many areas in our production facility where there was room for improvement. We are now satisfied users," says Oliver Marten, Swiss Krono Group

Production reliability 24/7.
The Swiss Krono Group is one of the world’s leading producers of engineered wood products and its facility in Heiligengrabe is one of the most successful manufacturers of OSB – oriented strand boards – in Europe. Other core competences at the site are the production of high-quality laminate flooring, medium and high-density fibre (MDF/HDF) boards and high-quality insulation material made of wood fibre.
To fulfil their customers’ demand for excellent quality and to meet their tight deadlines, the Swiss Krono Group is compelled to run the production systems 24 hours a day on almost every day of the year. Reliable cooling of electrical enclosures therefore plays a crucial role, as Frank Schmidt and Oliver Marten, Heads of electrical engineering in flooring manufacture and OSB departments respectively at the site in Heiligengrabe, explain:
“The maintenance staff have a lot of responsibility for ensuring that production runs smoothly at our site – day and night, on workdays and at weekends and on public holidays. The cost of production losses caused by machine downtime rapidly amounts to six-figure sums if we do not use the right technology, such as reliable cooling for our switching and machine control systems, of which we have many.”

Challenges of the wood processing industry.
Since the site in Heiligengrabe started up in the 1990s, many switching systems have been put into operation on the shop floor. They have been cooled up to now with filterfans and cooling units. The systems have frequently malfunctioned and production has even ground to a complete halt on occasion. Production downtime costs have resulted.
None of this is surprising, given the extreme conditions to which the switching systems in the wood processing industry are exposed. First of all, the air is contaminated with large amounts of dust. In some production areas, this is exacerbated by soot from the diesel engines in HGVs and forklift trucks.
Furthermore, heat and cold can also have a detrimental effect on technical systems under some circumstances. Last, but not least, there is a latent fire hazard: in wood processing, a short-circuit in the electronics can rapidly develop into a fire and therefore a serious risk in terms of safety and insurance.
This versatile thermal management concept allows us to shift considerable service capacity towards other tasks. We can respond to any requirement for maintenance and service with just a few replacement parts quickly and flexibly. That’s why we integrated Pfannenberg in our list of approved materials.
No maintenance and no dust.
The switching systems for a short-cycle press system at the Heiligengrabe site for producing flooring was fitted with twelve cooling units for electrical enclosures. Particularly in the summer, the extreme environmental conditions caused the plant to break down frequently: the control components overheated because the temperatures in the electrical enclosures were too high.
As there was water available for cooling in this workshop, Pfannenberg recommended the implementation of a thermal management concept with air/water heat exchangers with closed cooling circuits which would render them impervious to environmental conditions such as the dusty atmosphere or changing temperatures.
As a result, the existing cooling units for the electrical enclosures were replaced by air/water heat exchangers of Pfannenberg’s PWS/PWI series. These offer maximum reliability even at ambient temperatures of over 55 °C and in particularly polluted environments.
The air/water heat exchangers put a stop to the dust problem and the maintenance required was reduced almost to zero as, unlike in cooling systems, there were no condensers nor filterfans to require servicing. What’s more, the cooling system used 60 to 70 % less energy after the change to different technology.

Clean and clever: deluxe retrofitting.
Pfannenberg also modified a packaging line in the dispatch area of the production facility in Heiligengrabe where the finished goods are collected by HGVs. This area had also been plagued by breakdowns in the past due to the high levels of dust in the air. Previously, this switching system was cooled with ceiling fans and filters built into the enclosure doors to clean incoming air. First, Pfannenberg provided a deep-cleaning service for the whole switchgear cabinet, inside and out, including the PCBs on the inverters.
To prevent the cabinet from becoming dirty again and generating more costs as a result in the future, the ceiling fan combination was replaced by partially recessed, energy-efficient εCOOL DTI 6301 cooling units in combination with filterfans manufactured by Pfannenberg. These units are particularly suitable for use in higher ambient temperatures and in contaminated environments. For example, compressors with widely spaced fans prevent the deposit of dust and dirt and thus ensure that operation is reliable and maintenance at a minimum. The filterfans with their patented fluted filter mats have remarkably long maintenance intervals.

As part of the εCOOL range, the cooling units in the 6000 series also require up to 43 % less energy than traditional cooling systems and are equipped to be particularly service-friendly. Worn parts and other components can be replaced very quickly. A single technician can install or remove one of these units in about 10 minutes.


Cost benefits at maximum.
Cut-out compatibility was the crucial reason why the Swiss Krono Group chose thermal management solutions from Pfannenberg. This means that the air/air and air/water heat exchangers and the cooling units from Pfannenberg have identical housing cut-outs and fixing points.
Even the most recent devices in the energy-efficient εCOOL series are backwards compatible thanks to the standardised housing, so that older devices from the manufacturer can be replaced easily. It is now possible for one cut-out to be used for 11 different thermal management solutions.
Plant operators such as the Swiss Krono Group benefit from this in several respects. Identical housing cut-outs for almost every electrical enclosure bring standardisation to the service requirements and the stocking of spare and replacement parts. Another plus is the option to adapt the cooling technology quickly to changes in the environmental conditions, temperature and technology, which was the case in Heiligengrabe when the cooling units were quickly replaced by air/water heat exchangers.
“This versatile thermal management concept allows us to shift considerable service capacity towards other tasks. We can respond to any requirement for maintenance and service with just a few replacement parts quickly and flexibly. That’s why we integrated Pfannenberg in our list of approved materials,” explains Schmidt.
Consistent package solution.
The project in Heiligengrabe demonstrates the enormous importance of taking advice on thermal management for electrical enclosures. Without accurate analysis and extensive consultation on site with experienced experts, it is unlikely that these projects would ever have been implemented in the way they were and the considerable potential for optimisation would probably have remained unused.
It was the whole package of advice, service and technology that persuaded Frank Schmidt: “Our company is benefiting from the manufacturer’s know-how and carefree package. Obtaining advice, servicing and maintenance from a single source saves time and money.”
Summary
By implementing the Pfannenberg thermal management concept with its unique cut-out compatibility, the Swiss Krono Group at Heiligengrabe was able to reduce stocking and maintenance costs significantly. Furthermore the wood engineering company is benefiting from better machine and system availability thanks to greatly improved protection from dust. Using the energy-efficient εCOOL technology has also resulted in lower energy costs.
Facts at a glance.
Task
- Ensure the availability of machines and systems for wood processing at the Heiligengrabe site.
- Design a thermal management solution which would be impervious to dust-heavy atmosphere and reduce maintenance requirement.
- Develop a flexible thermal management solution which would guarantee rapid response times to breakdown and allow easy adaption to changes in the ambient conditions.
Challenges
- Protect sensitive switchgear from dust pollution.
- Stop switching systems from overheating and generally protect them from temperature fluctuations.
- Contain the latent risk of fire associated with wood processing.
Technique applied
- εCOOL cooling units (DTI/DTS series).
- Air/water heat exchangers (PWI/PWS series).
- Filterfans.
Success factors
- Compatible cut-outs guarantee rapid set-up times and facilitate warehousing.
- Easy retrofitting and upgrading thanks to cut-out compatibility and easily installed devices.
- Significantly lower maintenance requirement by replacing cooling units with air/water heat exchangers.
Descripción | Idioma | Tipo | Dimensiones | Descargar |
---|---|---|---|---|
Case Study Swiss Krono |
|
1,2 MB | Descargar |