very noisy. Multifunction LEDlights for industrial applications The QUADROLED-HI multifunctional light will also be on show on the Pfannenberg stand. This light is used for the visual signaling [...] Hamburg, 11 October 2017. At this year's SPSIPCDrives trade fair in Nuremberg, the electronics specialist Pfannenberg will be presenting communication-enabled thermal management devices for electrical [...] mechanical construction and categorization in high protection classes (IP66, IP67 and IK08), the QUADROLED-HI is suitable for indoor and outdoor use. PYRA® L: A powerful addition to the PYRA® series