Hamburg, 11 October 2017. At this year's SPSIPCDrives trade fair in Nuremberg, the electronics specialist Pfannenberg will be presenting communication-enabled thermal management devices for electrical [...] by forklifts, for example. This risk is avoided by the new position of the connections. An optional kit with cover panels is available with which to adapt the appearance of the PWI to the machine design
November 2017. Electronics specialists Pfannenberg will be presenting new air/water heat exchangers with a top-mounted water connection, and suitable for partially recessed positioning, at the SPSIPC Drives [...] recessing and the connection kit Model PWS 6502 T is designed for side-mounting and the PWI 6502 T version is designed to be partially recessed and side-mounted. A special kit with cover panels ensures [...] can be elegantly concealed with a connection kit. It can be configured both for the left and the right, or can be altered from top right to top left. The kit contains a cover with a bracket, quick-fit couplings