Casestudiesliquidcooling. We have numerous projects for clients from various industries successfully implemented. Here you will find concrete applications that will show you the importance of a consultative [...] exchangers cooling plastic caps on custom-made flat conveyors. Continue reading or download as PDF HPP Business Unit Chillers Application Liquidcooling solution for High Pressure Processing.The HPP is [...] management of control cabinets AND processes in corrugated cardboard packaging machinery. Watch the video TALENS Application: Thermal management of control cabinets AND processes in laser hardening machinery
Learn more about the basics of liquidcooling, as well as about products that meet specific requirements with superior reliability and efficiency. Casestudiesliquidcooling Solution examples from various [...] industrial liquidcooling applications. We are your partner for all questions regarding individual solutions for a wide range of industrial applications. We are happy to share our comprehensive know-how with [...] various customer projects and industry areas… Read more Packaged chiller solution Liquidcooling solutions with a closed water circuit offer significant benefits compared to traditional approaches… Read more
Company Application: Closed loop liquidcooling of electronics reduces downtime, maintenance & repair costs for commercial bakeries: Pfannenberg provides custom enclosure cooling solution for one of the fastest [...] Casestudies thermal management. We have numerous projects for clients from various industries successfully implemented. Here you will find concrete applications that will show you the importance of a [...] management of control cabinets AND processes in corrugated cardboard packaging machinery. Watch the video TALENS Application: Thermal management of control cabinets AND processes in laser hardening machinery
CaseStudy HPP – liquidcooling solution for high pressure processing. Pfannenberg EB 400 WT units to coolprocess fluids. Application. HPP Italia is the first Italian company dedicated to offer the food [...] digital alarm panel. Facts at a glance. Task Cool both process fluid and pumps for a high pressure processing machine. Application Food and beverage latest processing technology for safety without heat and [...] first one cooling the process fluid which is a 30 % glycol/water mixture to be brought from +4 °C to –1 °C with a flow rate of 4,500 l/h; – the second one is a refrigeration system aimed to cool down the
complete disposal to study together solutions for different types of applications . Please contact us! Energy conversion and hydrogen processing Energy conversion and hydrogen processing Hydrogen electrolysis [...] and longevity. The cooling system typically consists of a heat exchanger - that uses a cooling fluid such as water or air to dissipate the heat generated by the electrolysis process – and a chiller that [...] components that control the electrolysis process. Also these components can generate a significant amount of heat during operation, and in this casecooling can take place both by air - through filterfans
choice fell deliberately on the cooling units of the X-series from Pfannenberg. An X-Series cooling unit DTS 6X1E was mounted on the door of the control cabinet to cool the sensitive control cabinet e [...] of 70 cooling units realised within approx. 3 weeks Challenges: Realise significant savings potential Replacement of 70 cooling units during machine operation Product solutions: X-Series cooling units: [...] units: DTS/DTI 6X1E 230 V 7035 X-Series cooling units: DTS/DTI 6X2E 230 V 7035 Compact cooling unit DTS 6201C 230 V MC 7035 Top-mounted cooling unit DTT 6801 400 V MC 7035 Filterfan PF 43.000 IP 55 Exhaust
Casestudy A perfect package - Chillers cool down injection moulding machines at competence center Injection moulding requires very high temperatures, and the workpieces must be cooled down immediately [...] Systematic water cooling Now an EB 130 WT CE STD chiller with a cooling capacity of 12 kW at a maximum ambient temperature of 35 degrees is cooling the injection moulding processes of three injection [...] and competent partner, experienced in liquidcooling solutions. Fig. 5: The Pfannenberg cooling system for PolymerEngineering Facts at a glance Task Efficient cooling of several different injection moulding
CaseStudy MA DESIGN - Design experts recommend top-mounted cooling units. Clever design and functionality in machine and plant engineering. ma design is a think tank for innovative products, processes [...] is achieved mainly with an ingenious arrangement of the cooling circuits. Positioning the cooling components in the upper section of the cooling unit prevents the formation of a thermal bridge to the [...] 100 % condensate protection. Description Language Type Size Download CaseStudy MA Design Design experts recommend top-mounted cooling Units from Pfannenberg. English pdf 8.0 MB Download
CaseStudy Swiss Krono Group - It‘s all about the cut-out. Cut-out-compatible cooling solutions from Pfannenberg reduce maintenance requirements and improve machine availability for the Swiss Krono Group [...] operation for the packaging line. As part of the εCOOL range, the cooling units in the 6000 series also require up to 43 % less energy than traditional cooling systems and are equipped to be particularly s [...] the option to adapt the cooling technology quickly to changes in the environmental conditions, temperature and technology, which was the case in Heiligengrabe when the cooling units were quickly replaced
CaseStudy Custom chiller satisfies temperature control in chemical synthesis reactor. Pfannenberg fits chiller into confined space within a packaged Ferrator ® targeted for water and wastewater treatment [...] Ferrate Treatment Technologies, LLC of Orlando turned to Pfannenberg for help with developing a liquidcooling solution for a small, cabinet based system. While already using Pfannenberg chillers for larger [...] homogenizer and reaction chamber. The final product is a liquid which is stored in a tank. Both the reaction and storage areas require cooling, which is provided by Pfannenberg chillers. Pfannenberg open-frame