Background lighting can degrade the visibility of the warning signal. A blind can be mounted in the interior of the light to reduce the transparency of the lens and block background light, thus achieving better contrast levels for the warning signal. Two installation positions, set off at 90° from one another, are included for optional blocking of lateral light.

The blind must be ordered as a separate accessory.

Article number: 28112000039 (Pack of 5)