UL chillers

UL option now availaible for Pfannenberg chillers. Another step in our continuous commitment to quality and supporting our international OEM customers.

UL chillers

Compliance with UL standards is an optional and globally recognised accreditation and a standard Pfannenberg has chosen to conform to, showing our continued commitment to quality and supporting our international OEM customers. UL certification can only relate to some aspects or equipment of the machine, depending on the standard applied. For example, it is common to carry out the certification of only the electrical panel of the machine according to the UL 508A standard.

What is UL 508A?

The standard provides guidelines to panel builders on various issues including component selection and wiring methods. Only panels constructed to meet the full construction requirements and recommendations defined in UL508A can be labelled as such. And UL508A, along with a whole list of other standards, are set by Underwriter’s Laboratories - a US-based safety and certification company.

A huge opportunity to export to U.S.

In 2019, the #1 EU export products were machinery and equipment (13.0 % of total exports), while machinery, excluding electrical and computer equipment, was the second-largest component of EU imports for the U.S. at $75.6 billion.
[source Eurostat]

We are well aware of how important it is that each component respects the technical specifications imposed by this market.
That's exactly why Pfannenberg is among the few suppliers to have introduced a full range of UL-certified chillers into their product portfolio.

24/7 on site service

Pfannenberg not only offers a range of UL-certified chillers for export to the U.S. and Canada, but does so as a manufacturer with a U.S. base of operations. This means we are able to provide on-site installation and maintenance service 24/7.

Pfannenberg Services provides a wide range of offerings that enable you to enjoy the highest levels of performance from the systems in your factory or facility. Weather you’re installing new equipment, maintaining an existing system or completely upgrading your infrastructure, Pfannenberg on-site Services and consulting can provide exactly the expertise you need. We will customize programs to meet your budgetary demands.