Machine safety (PL)

The objective of EN ISO 13849-1 and EN 62061 is to minimise the risk in operation of machines. Find out more about risk assessment and how it affects the use of visual and audible signaling devices.

Functional safety EN ISO 13849-1 (PL)

Safety Instrumented System SIS (safety loop)

Two safety standards became effective with the machinery directive. On the one hand, EN ISO 13849-1, which replaces Norm EN 954-1 of the old machinery directive 98/37/EG. On the other hand EN 62061.

Objective of these safety norms is to minimise risks in the operation of machines. Therefore, the requirements for the certification of products for machine and plant manufacturers were increased.

Probability considerations, amongst other things, have an impact on the regulation of the safety of components.

In order to keep the existing residual risk of a machine or plant as low as possible, alarm devices which have a high functional safety are required. They should also alert about danger via visual or audible warning signals.

A hazard graph is not only an important element for the classification of the system or plant, it also clearly illustrates how complex the preliminary work is for the realisation and implementation of projects.

Risk assessment

Risk parameters

S – Severity of the injury     

  • S1 = minor injuries (normally reversible)     
  • S2 = serious injuries, including death (normally irreversible)

F – Frequency and/or length of exposure to the hazard     

  • F1 = rarely to more often and/or short periods     
  • F2 = frequently to continuously and/or long duration

P – Possibilities to avoid danger     

  • P1 = possible under certain conditions     
  • P2 = barely possible

Publications / Applications

Description Language Type Size Download

SIL/PL fundamentals for machine technology

  • English
pdf 5.7 MB Download

Control example „Machinery Start-up“

  • English
pdf 270 KB Download

Control example „Muting Operation“

  • German
pdf 430 KB Download

Brochures / Poster

Description Language Type Size Download

Facilitate norm-conforming Functional Safety

2-page A1 poster

  • English
pdf 2.5 MB Download

Safer running of processes and risk minimisation

in the operation of plants and machines Safety-related sounders and flashing lights (Edition 15)

  • English
pdf 1.1 MB Download

Functional Safety info sheet

EN ISO 13849-1 (PL)

  • English
pdf 1.0 MB Download

Software assistant SISTEMA

Control safety of machines – easily calculated.

The manufacturer-independent calculation tool SISTEMA, from the German Occupational Health and Safety Department (IFA) helps by the evaluation of safety-related control systems according to EN ISO 13849-1 and simplifies risk analysis.

For further information and to download the Pfannenberg SISTEMA library please click here.